Part Number: MSP430-IEC60730-SW-PACKAGE
Hi,
We are using MSP430 IEC60730 software package. For class B compliance, do we need to run both POST() and PST() tests or one of these is enough?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430-IEC60730-SW-PACKAGE
Hi,
We are using MSP430 IEC60730 software package. For class B compliance, do we need to run both POST() and PST() tests or one of these is enough?
Hi Akash,
We provided some IEC60730 example here, for which function you need to test, maybe you can try to consult with certified manufacturer。
Thanks!
Best Regards
Johnson
**Attention** This is a public forum