Hi,
1.I try to change the project name that time the below mentioned error would come ,Now what I do?
2. And also copy the project and paste it to another workspace that time also error occur?
Description Resource Path Location Type
#16019-D file "../lib_msp430_v2.0.0_iaq2_.0.0/msp430fr5043_iaq_2nd_gen.lib<iaq_2nd_gen_V6_nnet.c.o>" specifies small code memory model, which is not compatible with large code memory model specified in a previous file or on the command line aqm_v2.0.1 C/C++ Problem