This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Our board manufacturer is using Elprotronic FET-Pro430 and MSP-FET430UIF to program a MSP430F6726 via Spy-Bi-Wire. He is asking why it takes almost two minutes to erase and reprogram the flash memory. He updated the memory options page to include just the areas being used but that does not help. The application is less than 24K and when I program the application using the IAR tools it does not take that long. Thank you for any assistance you can provide.
JB
Hi James,
What's the SBW speed setting in the Elprotronic FET-Pro430?
Could you help to provide the log file when doing the firmware program?
**Attention** This is a public forum