Other Parts Discussed in Thread: MSP430FR2633, , CAPTIVATE-BSWP, MSP430F5528
Hello,
I am looking to test out the performance of the TIDM-1021 evaluation board. To this end I built a PCBA based off the hardware design files and ordered in the CAPTIVATE PGMR. I downloaded the TIDCET6 software package and generated the IAR code through CapTIvateDesignCentre, but when I programmed the MSP430FR2633 none of the LEDs would light up.
While running the project with CapTIvateDesignCentre allows me to see which button is pressed, it appears that the actual code running on the MSP430FR2633 is more closely related to the CAPTIVATE-BSWP Firmware. This can be seen through the main.c and CAPT_BSP.c files, as the TIDM-1021 does not set up the right I/O for its peripherals but instead sets up for those of the BSWP.
Has anyone found the right files to use with the TIDM-1021 evaluation board?
Thanks