Hello,
I have a question about MSP430 clock initialization
The file name I am referring to is "msp430fr243x_CS_03.c".
・How was the value (487) in the following code determined?
CSCTL2 = FLLD_0 + 487; // DCOCLKDIV = 16MHz
Next, we referred to the following file.
---msp430fr267x_CS_05.c
The frequency is the same at 16MHz setting, but the Software_Trim function is executed.
The execution time of Software_Trim function is about 70ms.
・I do not want to execute the Software_Trim function, is this a problem?
best regards