This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5043: MSP430 temperature sensor

Part Number: MSP430FR5043
Other Parts Discussed in Thread: EVM430-FR6047, , MSP430WARE

Hi !

I am currently using EVM430-FR6047 and I am going to design a board with MSP430FR5043
I want to add a temperature measurement option.

I saw in:
MSP430FR604x, MSP430FR504x 16-MHz MCU up to 64KB FRAM, 12-Bit High-Speed ​​8-MSPS Sigma-Delta ADC, and Integrated Sensor AFE datasheet (Rev. B)
That should connect somehow with the ADC12

Can I get a recommendation on how to connect a temperature sensor to the MSP without adding more hardware?
Which sensor is recommended?

**Attention** This is a public forum