Other Parts Discussed in Thread: MSP430F2274, CC2500
Hi,
I'm developing a projecto and I'm using the MSP430F2274 as main core. I have a microSD card and a MP3-Decoder connected to my MSP through SPI. I can manage individually without any problem the microSD card and the MP3-Decoder, I can manage with any problem the microSD card and the MP3-Decoder with the same SPI port (SPI-B), but I can't try to manage the microSD card through the SPI-A and the MP3-Decoder through SPI-B, because they don't works well.
I asking myself If is it posible to use both SPI modules in MSP430F2274?
Thanks for all.
Regards.