Does the MSP430F55xx USCI I2C state machine function as a master require an ACK from the slave for it to run continuously? I have only one MSP-TS430RGC64USB eval board. What do I need to change in the MSP430F55xx_uscib0_i2c_06 (or MSP430F55xx_uscib0_i2c_08) from the slac300d.zip example codes to have configure the I2C running in master TX mode without a slave connect to it? No ACK from the slave.
I am in the process of getting a second MSP-FET430U64USB eval board to use it as an I2C slave. The second board will use the MSP430F55xx_uscib0_i2c_07 (or MSP430F55xx_uscib0_i2c_09). What do I need to do to connect these 2 boards other than have 10K pull up on the P3.0 & P3.1 signals as described in the code?
Thanks in advanced.
Sy