Other Parts Discussed in Thread: TIDA-01486, THS3095, MSP430FR6047
Tool/software:
We are attempting to use the TIDA-01486 amplifier with the EVM430-FR6047 in order to evaluate the TI ultrasonic platform with metal pipes. I am having the worst time trying to get this system working.
First, I am using only 1 pair of transducers. I have cut the following traces from J1 and J2 of the TIDA-01486 design: S1, S2, S3, S4, PD1,, and PD2. Then I have hardwired these signals in accordance with the table 2 of TIDUDO7 (TIDA-01486 User Guide). Since I am using only 1 pair of transducers these signals don't need to be switched so hardwiring them should use Pair 1 all the time. I have assumed that a 1 in Table 2 means to tie that signal to 3.3 V, and a 0 in Table 2 means to tie that signal to GND.
I have connected the jumpers on the EVM430-FR6047 on J30 which makes the EVM430-FR6047 supply 3.3 V to the TIDA-01486 to power the switching components. And I have connected a jumper to J6 of the TIDA-01486 which tie the 3.3 V rail to the Vbias signal for the receive path.
For the external +/-15 V power supply, I am using 2 BK Precision 1550 power supplies, each set to 15 V and connected in series with the mid voltage point tied to chassis ground as shown in the folling picture:

The power up sequence I have to use is to turn on the external +/-15 V power supplies at the same time, and then I plug my laptop into the USB connector on the EVM430-FR6047 and connect the USS software to the EVM. This sequence is the only way that I can power everything up and still be able to connect the USS software to the eval board.
The problem I am having is that there is no ultrasonic transmit signal. And U5 and U6 (the THS3095D op amps in the CH0 and CH1 receive paths, respectively) are getting really hot. The current drawn from the 2 external supplies is 150 mA. This seemed high to me at first, and I guess since the op amps are getting hot it probably is high. The external +/-15 V supply is only powering 4 of the 8 op amps so the external supplies should only be drawing about 40 mA each. U5 and U6 are both enabled by control signal PD1, which is a 1 in Table 2 and I have connected to 3.3 V.
Am I using the correct power up sequence? Obvioulsy, you can't debug my system, but do you have any ideas what could be wrong? I have double and triple check my trace cuts and the jumper wires I have added. Any help would greatly be appreciated.