This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
Currently i am doing migration of code from the Code Composure studio to the IAR. I am using msp430f5418 for my application. I am successfully able to build and load the firmware into the chip by using the JTAG. But i am not able to get it working with the msp430-txt file created by the IAR. Where as the msp430-txt file created by the CCS is working fine. When i went on debugging i found that msp430-txt file created by the IAR is not able to upgrade into the chip successfully. It has failed to download at the addreass location of 0x7AF0. does anybody came across such situations ? or if anybody knows what are i can try in the options provided by the IAR.
Thanks & Regards
Aloka Hegde
**Attention** This is a public forum