Tool/software:
Hi All,
My customer have a question about the .dll I got from E2E below.
As I am a colleague of GR, I ask the question instead.
They are developing in CUI, not GUI.
They have tried the file I gave them in CUI,
still cannot write the program to MSPM0G1105 successfully.
The MSP-GANG.exe (GUI tool) can write to MSPM0G1105 successfully,
At this time, They have changed the project setting to “File” ⇒ “Save Project As...”. (mspm0g1105.mspgangproj).
LONG MSPGANG_Load_Config loaded the project into CUI, but could not write it.
What is the cause of not being able to write in CUI?
Also, currently the sample code for the CUI tool is DLLtest.c.
"C:\Program Files (x86)\Texas Instruments\MSP-GANG\Examples\C_Applications _MSP_DLL"
This code uses the MSP430F2121 as an example device, is there any sample code using the MSPM0G1105 as an example?
Best Regards,
Ito
Hi Ito,
I've reached out to our tools expert who has an example for MSPM0 devices. Please take a look at the examples listed under C:\Program Files (x86)\Texas Instruments\MSP-GANG\Examples, in this directory you should be able to find multiple examples including one for MSPM0. Let me know if you are able to find these or if you require further assistance.
Hi OBrien,
Thank you for your reply.
Customer is already looking at C:\Program Files (x86)\Texas Instruments\MSP-GANG\Examples.
What is the sample code for the CUI tool for the MSPM0G1105?
If not, please let me know why.
Best Regards,
Ito
HI KZ,
My colleague sent me Program_tool.zipthis file, and mentioned this is found in that file directory as well. He mentions that you will need Visual studio in order to build it.
Hi OBrien,
I still cannot find the sample code for MSPM0G1105.
Can you give me the specific directory and file name?
Best Regards,
Ito
Hi KZ, it looks like the example is found under Program_Tool\C_Applications_MSP_DLL\DLLtest.c
Hi OBrien
Thnak you for your reply.
How can I modify an MSPM0L1306 file to create an MSPM0G1105 file?
Best Regards,
Ito
Just replace the MSPM0L device with the device you are using it is plug and play
**Attention** This is a public forum