Tool/software:
I'm having trouble connecting to the EVM430-FR6047 with the USS GUI. I keeps throwing this error every time:
"more than one HID device with the same VID/PID detected. Only one device may be connected"
I am using windows 11, but I can't figure out any issues on my computer side. I have installed and uninstalled the driver, the GUI, and I have tried to deselect COM Ports so that there is only one active at a time, but still no luck.
Below is the com ports that I have for the board:
Also when I try to "Load Image" it successfully loads the program.
But when I try to "Verify Image" it fails. I also tried to erase all the flash and reprogram, but the same issue occurred.
This is my set up for hardware:
Hi,
It should relate to USB driver issue. I would suggest to use 3rd party tools like USBDeview to uninstall the useless USB driver on your computer and then try again.
Best regards,
Cash Hao
how do I know which drivers are useless?
Here are the HIDs and the communication interfaces, I have tried disabling certain ones but all are still failing in the same way except when I disable this one
It shows no match hardware interface found.
Hi,
Well, I do not have much advise on this topic. I would suggest try on a different computer and check if you observe the same issue.
Best regards,
Cash Hao
**Attention** This is a public forum