Hi,
I have 2 analog signals , one is the battery voltage(signal 1) and other is a device specific signal (signal 2).
They are fed into P6.4 / A4 and P6.5 / A5 of the microcontroller .
The conversion of both the signals will be initiated by the user at different times.
when the user says "Get me the battery voltage" , the conversion for the signal 1 has to happen .
when the user says "Get me the intensity of signal 2 " , the conversion for the signal 2 has to occur .
But I understand that ADC12SC starts the conversion for both the signals in one stretch .
Is there a way to control which signal/input channel has to be converted by the ADC ?
Please comment / correct me if i am wrong .
Thanks in advance ,
Jenitta