I've got a custom MSP430F5519 board which uses a TPS61220 to provide power from 4 x AA (in parallel, is an option to power from a 24VAC using an LM317.)
The DCO is used to generate a 4MHz clock from XT1 (32KHz) on SMCLK.
I'm implementing a simple single-slope ADC using comparator-B and timer-A0 clocked from SMCLK. When power from AC, the ADC samples within 0.1%; however, when powered from batteries, samples jitter +1%. Using a scope, VCC seems clean.
Any ideas on what I should look at next?