Have been using the same FET (for some reason it is marked as a MSP-FETU430IF for more than 1 and half year but it stopped working this morning.
Followed all the advice I could find on the forums, reinstalled drivers, removed driver and plugged in FET as "new" device, removed registry entries, changed com port enumeration, closed all applications on PC and used Process Explorer to check if anything was holding the com port.
The device operate as normal, flashing Red LED followed by green LED staying on, device is properly picked up on Windows XP and correctly installed.
When trying to program a CC430 after the binary has been compiled an "Error initializing emulator: No USB FET was found" is displayed.
When trying to upgrade or downgrade the FET with the firmware update utility it stays on "0% Initializing bootloader ...".
When trying to program the CC430 with the Elprotronic Lite application the following error pops up, "The FET-Pr430 free version works only with Texas Instruments' FET adapters.If the 3-th party FET adapter is used then the standard FET-PRo430 should be used.
I then retrieved the back up FET from the cupboard and it works on the same setup.
The original FET seems to be in good working order hardware wise, is it possibly bricked (do not know how since it hasn't been upgraded/downgraded in the last 9 months)?