Hello,
As of my experience so far uptil this morning, assume I put a breakpoint at line 100 in a source file, and I press F8. But if for some reason, control is stuck before this line 100, and if I press the double bar (||) button to stop execution, then the line at which the control is stuck will be highlighted by the debugger, and the debugger will take me to this line, even though this line may be in a different source file.
But as of this afternoon, when I press the double bar button, then the debugger does not stop at the line at which control is stuck. And it gives no indication where it is. So I have no way to find out where the control is stuck.
I did not change any settings of the debugger. I rebooted the PC twice.
I highly appreciate if you could point out what I should do to bring back the behavior of the debugger, i.e. the debugger should stop at the line at which the control is stuck, when I press double bar button.
BTW: start of F8 is pressing F8, and stop of F8 is pressing the double bar button.
Waiting for your response!!!!!!
Babu