- Objective: Trying to utilize the SD16 module to sample signals from 8 - 12 Khz at 32Ksps (using OSR32)
- Board: MSP430FE427
- MCU
- MCLK: Approx 8Mhz (using FLL & ACLK)
- ACLK: 32 Khz
- SD16
- Fm: MCLK / 8 (approx 1 Mhz)
- OSR32 - To provide close to 32Ksps
- UART
- Baudrate: 921600 (U0BR0 = 0x08; U0BR1 = 0x00;)
- I use the UART to send data as fast as possible to the PC, to do some quick Frequency analysis to verify the preformance of the SD16.
- Question
- Can someone tell me if anything like this has been done using any of the MSP430?
- I seem to be having a lot of issues and not seeing the expected results or performance from the SD16 or MSP430 module.