This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi;
I am using MSP430FR5739 Experimenter's Board. RTCCLK is configured to output at a frequency of 1 Hz . I measured RTCCLK is 1.0000279 Hz. This frequency error is approximately 27.9 ppm too high. To decrease the frequency by 27.9 ppm, RTCCALS is cleared, and RTCCAL is set to 13 (27.9 /2.17).
My code is :
RTCCTL23 |= RTCCALF_3;
RTCCTL23 |= RTCCAL3 + RTCCAL2 + RTCCAL0;
P1DIR |= BIT0;
P1SEL1 |= BIT0;
I calibrated RTCCLK, measured RTCCLCK again. RTCCLK result is 1.0000279 Hz.
My questions is :
Can I see effect of the calibration in the period of 1 sec? or Can I see effect of the calibration in 1 hour?
MSP430FR5739 user guide says;
"""Each RTCCALx calibration bit causes either 256 LF crystal clock cycles to be added every 60 minutes or 512 LF crystal clock cycles to be subtracted every 60 minutes, giving a frequency adjustment of approximately -2 ppm or +4 ppm, respectively. """
What exactly is described in the above sentence. How the calibrated signal is observe at the end of the calibration
Thanks and greetings,
Murat Çelebi
Murat Celebi said:Can I see effect of the calibration in the period of 1 sec? or Can I see effect of the calibration in 1 hour?
Murat Celebi said:""Each RTCCALx calibration bit causes either 256 LF crystal clock cycles to be added every 60 minutes or 512 LF crystal clock cycles to be subtracted every 60 minutes,
So each hour, there will be a shorter or longer second. Once.
Internally, I guess (though I do not know), the hardware will add the calibration to the prescaler when the minutes roll over (for a shorter second) or something like this.
**Attention** This is a public forum