Hi All,
I am using MSP430F5501 controller for low power application in this we are using two GPIO pins 1&2 which are also multiplexed with coparator B.Comparator B have four channels in which two channels are connected to these GPIO pins 1 and 2 and others are connected to another two I/O pins 3 and 4.We are using comparator for these 3&4 pins but we are not using 1&2 pins for comparator even though comparator is turning ON automatically for these 1&2 pins and consuming energy and affecting these GPIO pins as well.So can anybody tell me why this is happening without using those pins for comparator?