Hi
I am using MSP430F5635 MCU .
1. Can I use one instance of Timer A to count 2 differnet intervals .
eg. I want to get an interrupt when the timer counts 1500 ms and another interrupt 1200 ms .
How should I configure the timer for that ?
2. In the above case , both the interrupts are overflow interrupts or Capture/compare interrupts ?
What is the difference between both Interrupt types ?
Thanks !
Jenitta