This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue with TIMER1_A0_VECTOR on msp430f5528 trying to create PWM on TA1.0

Other Parts Discussed in Thread: MSP430F5528

I'm having a issues with the ISR function being called.    I'm using examples based from this document slaa513.pdf

I put the timer into continous mode (MC_2) and enable the interrupt (TAIE) and trying to use SMCLK (TASSEL_2)

The problem is it freezes, sometimes it goes into the the interrupt routine other times it does not. 

if I use TASSEL_1 it will work for a while and then freeze.  I have tried setting up the SMCLK it a couple ways but it doesn't see to help.  And if I create a PWM using MC_1 on TA1.1 to create a PWM it works fine using SMCLK.   

Is there something simple I'm missing here?

Code pasted below.. Note how I'm trying to vary the duty cycle using the servo1_value var in a simple loop.


#include <msp430f5528.h>

// SERVO 1 connected to P1.7/TA1.0

#define     PWM_SERVO1_BIT BIT7 //P1.7

#define     PWM_SERVO1_DIR P1DIR // Each Servo uses the different DIR,SEL,OUT

#define     PWM_SERVO1_OUT P1OUT

#define     PWM_SERVO1_SEL P1SEL

#define PWM_SERVO1_TxCCR TA1CCR0 //Timer A1 TA1.0

#define PWM_SERVO1_TxCCTL TA1CCTL0

#define PWM_SERVO_TIMER_CONTROL TA1CTL

#define PWM_SERVO_PWM_PERIOD TA1CCR0

#define PWM_SERVO_MIN   250 // old values

#define PWM_SERVO_MAX   500

#define PWM_SERVO_PERIOD   500

// LED defines for bits and outputs.

#define     LED_RED_BIT BIT7

#define     LED_BLUE_BIT BIT6

#define     LEDS_DIR P6DIR

#define     LEDS_OUT P6OUT

// LED ON/OFF Commands.

#define LED_RED_OFF LEDS_OUT &= ~LED_RED_BIT

#define LED_BLUE_OFF LEDS_OUT &= ~LED_BLUE_BIT

#define LED_RED_ON LEDS_OUT |= LED_RED_BIT

#define LED_BLUE_ON LEDS_OUT |= LED_BLUE_BIT

#define LED_RED_CYCLE LEDS_OUT ^= LED_RED_BIT

#define LED_BLUE_CYCLE LEDS_OUT ^= LED_BLUE_BIT

unsigned int servo1_value = PWM_SERVO_MIN;

void main(void) {

WDTCTL = WDTPW+WDTHOLD; // Stop that silly watchdog timer

// init the ports for setting up the LEDS

LEDS_DIR |= LED_RED_BIT + LED_BLUE_BIT ;  // Set LEDS to output direction

LED_RED_OFF; // start with LEDS OFF

LED_BLUE_OFF; // start with LEDS OFF

PWM_SERVO1_DIR |= PWM_SERVO1_BIT; // setup output direction

PWM_SERVO1_SEL |= PWM_SERVO1_BIT;  // set timer to update this output

PWM_SERVO1_TxCCTL = OUTMOD_4 + CCIE; // enable interrupt

PWM_SERVO_TIMER_CONTROL = TASSEL_2 + MC_2  + TAIE;  // set SMCLK, continous mode, and interrupt enable.

__bis_SR_register(GIE); // enable interrupts

int pos = 0;

int i = 0;

while(1) {

     pos = 240;

     for(i=0;i<=25;i++) {

          pos = pos + 10; // increment for testing purposes

          servo1_value = pos;  // update the duty cycle for the ISR function below

          __delay_cycles(100000); // delay between PWM duty cycle changes.

          LED_BLUE_CYCLE;

     }

}

}

#pragma vector=TIMER1_A0_VECTOR

__interrupt void TIMER1_A0_VECTOR_ISR(void) {

     LED_RED_CYCLE;

         if(TA1CCTL0 & CCI) // If output currently high

         {

              TA1CCR0 += servo1_value; // PWM high  ( this value plus the "else" value needs to equal pwm period.

         } else {

              TA1CCR0 += PWM_SERVO_PERIOD - servo1_value; // PWM low

         }

}

  • I cleaned up the code above...  Hopefully that makes it easier to read.

  • Hi,

    if I have understood correctly, you want to generate a PWM signal with TA1.0.

    I do not have worked with this device in particular, I work with F5438A, both devices share  family, I am going to try to give you some advices:

    - TIMER1_A0_VECTOR_ISR shares the interrupt routine for the compare register reached by the timer (TA0R = TA0CCR0) and for the timer overflowing. So you only have to enable CCIE of CCR0 register, but not the TAIE. If both are enabled, the code will enter in the ISR for two conditions, and I think that you only want to enter when the timer reaches CCR0.

    - I do not know the pinout of that uC, but maybe, the output can be sourced to different pins. Check in the datasheet, if TA1.0 work as second function in more than one pin. If it happens, you have to select the pin you want to use as output, for this, in the compare register control register (TA0CTL0) you have to configure the CCIS bits.

    With this advices I get generate a PWM by easy way. Some name register can be wrong, so check them to ensure.

    I hope it helps you

  • Thanks T Da,  

    After removing TAIE, I'm getting much better results.  It looks like if I enabled both ISR conditions it was locking up.

  • Regarding not using TAIE.  In the example in the pdf linked in my first post, they show the following.

         TACCTL0 = OUTMOD_4 + CCIE;
         TACCTL1 = OUTMOD_4 + CCIE;
         TACCTL2 = OUTMOD_4 + CCIE;
         TACTL = TASSEL_2 + MC_2 + TAIE;

    Does this mean the  g2452 handles this differently?   Or is the ISR called twice and somehow can handle this without a issue?  Just curious.  I'll have to test this later on a lauchpad when able.

  • c_builder said:
    #define PWM_SERVO1_TxCCR TA1CCR0 //Timer A1 TA1.0


    This is somewhat dangerous. It suggests that you can change the used CCR just by changing this define (and hte related ones). However, the TIMER1_A0_VECTOR will only handle this specific setting. Anything else won't work.

    The whole thing will fail if either the high or the low part of the PWM output is below a certain threshold (depends on timer speed and CPU speed). Imagine what happens if servo1_value is 0? Right, you're adding 0 to TA1CCR0. This means, the next interrupt will be triggered after a full timer cycle of 65536 ticks. You won't be able to change the DC for that amount of time. This will happen for any step size that is smaller than the timer ticks that pass while executing the ISR.
    Maybe this is not critical in your current application, but maybe it is.

    The missing ISR for the timer overflow (TAIE) or superfluous TAIE bit has already been discussed.

**Attention** This is a public forum