This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi! All
We are trying to write some data to serial port using the code below
P3SEL |= 0xC0; // P3.6,7 = USCI_A1 TXD/RXD
UCA1CTL1 &= 0x00; // Clear register
UCA1CTL1 |= UCSSEL_1; // CLK = ACLK
UCA1BR0 = 0x03; // 9600 (see User's Guide)
UCA1BR1 = 0x00; //
UCA1MCTL = UCBRS_6; // Modulation UCBRSx = 3
UCA1CTL1 &= ~UCSWRST;
while (!(UC1IFG&UCA1TXIFG)); // USCI_A1 TX buffer ready?
UCA1TXBUF = err_code; // TX -> RXed character
while (!(UC1IFG&UCA1TXIFG));
We are getting data in UCA1TXBUF but its not pushed out to the serial port.
Please help us.
Thanks
Did you switch the port pin from GPIO mode to module mode (using PxSEL register)? If not, the port pin is in GPIO mode and won't output what the USCI module generates.
**Attention** This is a public forum