This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using CCS version 5.3 and MSP430F169 micro. I'm trying to load a custom bootloader and main application program into memory using the debugger. I need to use interrupts in both the bootloader and main application so I've remapped as follows.
Bootloader reset/int vectors 0xFFFF - 0xFFE0
Bootloader program code 0xFFDF - 0xD800
Main reset/int vectors 0xD7FF - 0xD7E0
Main program code 0xD7DF - 0x1100
For both projects I've altered the Debug Configrations->Target->Download Options to be "Erase and download necessary segments only. To prevent the debugger from erasing the entire contents of flash.
I then program the main application code first and then the BSL program. When running the debugger I can't step through the code? When I look at the flash contents I can see both programs are in code? Note in the linker script files I've only changed the FLASH and RESET/INT vectors to the appropriate locations and sizes. Is there something I'm missing?
My goal for this exercise would be to have both programs loaded with the main reset vector pointing to the BSL and executing first and then jumping to the main application code. I'm planning on having the BSL own the reset and interrupt vectors and having it re-route interrupt requests depending on which program is currently executing.
Any help would be greatly appreciated.
Regards,
Dan
How do you 'tell' the MSP to use the main reset/int vectors?
It's nice that you told teh linker to put them elsewhere, btu the MSP doesn't care for linker scripts. It always takes the vectors from 0xffe0+.
How does your bootloader call your application?
Hey Jens,
Keep in mind that I'm new to MSP430 development and have never gone into this level of detail on the linking and execution of the code before. I can appreciate that there are many different ways to develop a custom BSL application so in posting here in the forums I'm hoping to not only enhance my knowledge on a particular approach but also to get some advice on some other approaches.
So for my current approach my plan is to have the bootloader application "own" the reset and interrupt vectors at 0xFFE0. On startup the bootloader app would execute by default. The bootloader application will check a flag residing in flash (probably inside the information section of flash at 0x1000). This flag will tell the bootloader whether to jump to the main application (residing at 0x1100) or to remain in the bootloader and wait for a programming command over I2C. In the bootloader, the interrupt handlers will all check this bootloader flag as well and either execute the bootloader handler or jump to 0xD7E0 to where the main application interrupt handlers reside. This will add latency to the handlers but shouldn't be an issue for this application.
As mentioned, I'm interested in feedback on this approach to a custom bootloader and alternative approaches, but my original post was more on some IDE configuration issues and how to get multiple programs loaded and running using CCS. When I load the main application first and then the bootloader application (with no jump right now) I'm not getting anything happening on startup. I'm using the debugger interface on CCS to load the programs. Is there a separate stand-alone programming utility that has more control on how and where to program things into flash. I still think there is a gap in my understanding of how the MSP430 builds, links, and programs code.
I appreciate any assistance.
FineDan Closson said:So for my current approach my plan is to have the bootloader application "own" the reset and interrupt vectors at 0xFFE0.
Fine.Dan Closson said:On startup the bootloader app would execute by default. The bootloader application will check a flag residing in flash (probably inside the information section of flash at 0x1000).
Not so fine. YOur assumption that the code entry point is 0x1100 is only valid if your application is a non-relocatable assembly application. In any othe rcase, the linker will set the entry point location based on a lot of factors. That's why there is such a thing as a reset vector instead of just running from start of flash.Dan Closson said:This flag will tell the bootloader whether to jump to the main application (residing at 0x1100) or to remain in the bootloader and wait for a programming command over I2C.
Same problem. But by 'moving' the interrupt vector segment in the linker script to this location, it is safe to expect the vectors there. But why 0xD7E0? Is your bootloader so large that it needs the area from 0xD800 to 0xFFE0?Dan Closson said:In the bootloader, the interrupt handlers will all check this bootloader flag as well and either execute the bootloader handler or jump to 0xD7E0 to where the main application interrupt handlers reside.
But you're right, for these ISR that the bootloader uses, you'll need to check whether the bootloader is active or not. And you need to disable these interrupts before you call the application. However, in most cases you can as well do a polling of the peripherals and do not need any interrupts at all inside the bootloader.
Of course you can store multiple applicaitons in an external memory and load them through your bootloader from memory into flash as required (e.g. select by a jumper settign on GPIO pins). When started, teh loader checks the currently loaded application and compares it to the jumper settings on soem port pins. If it matches, fine, if not, it loads the 'proper' application from external memory. THis allows for a multi-purpose device even if not all applications fit into the internal flash into a 'super-application'.Dan Closson said:my original post was more on some IDE configuration issues and how to get multiple programs loaded and running using CCS.
However, loading an application from external memory takes quite some time, and power.
**Attention** This is a public forum