This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Let me explain what I meant.
Suppose there was no such bug (or TI fixed that bug), CPU or DMA must pickup RXBUF within about 8 I2C clocks. Otherwise there will be problems.
Now, with this bug, CPU or DMA must pickup RXBUF within about 7 I2C clocks.
Thus, you only need to be 8/7 = 115% as fast to avoid this bug.
Hello old_cow
The thing is that here it is happening in LPM0 (CPUOFF) within an interrupt
and (and per guide) the usci forces the DCO clock on (since smclk is sourced from there and the usci from smclk).
The DCO in this exemple is running at 1MHz, the SMCLK @ 500khz (/2) and the usci @ 50khz (smclk/10)
The thing is that in LPM0 i have no idea at what frq is running the component that takes care of the interrupts...
Hey, surprise surprise,
just posted my problem here which is maybe the same as yours. Do you also have problems in master-receiver-mode? The second byte is aborted in my application which sounds like USCI30 from the errata. Maybe you could read my post, too? Is it an identical error?
http://e2e.ti.com/support/microcontrollers/msp430/f/166/t/273974.aspx
Dennis
An interrupt switches MCLK on which in turn activates its source (which is already still on in your case), so execution of the interrupt begins with the next MCLK cycle.JeGeVa said:The thing is that in LPM0 i have no idea at what frq is running the component that takes care of the interrupts...
**Attention** This is a public forum