This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
All,
I'm going through the
MSP-EXP430F5529 Experimenter Board User Guide
I plugged in the programmer and got a green LED. Then I made it this far:
"You may be prompted to update the firmware on the MSP-FET430UIF programmer. Do not be concerned;
click the button that says Update, and the program download should continue as expected."
At this point it hung. After about an hour I rebooted, now I'm not gettting any LEDs.
I'm getting this error:
MSP430: Error initializing emulator: Could not find MSP-FET430UIF on specified COM port
I'm using Code Compiler v5.4 with a MSP-FET430UIF.
My Device Manager shows:
MSP-FET430UIF - VCP (COM6)
Any suggestions?
thanks,
Scott
Hi Scott
1) Do you have adjust the SW for correct setting?
Please see the Figure 8.
2) Could you can check your connection of CCS properties?
Best Regards,
**Attention** This is a public forum