This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
while debugging in the debug mode iam getting this error message.
MSP430: AutoRun: Target not run as breakpoint could not be set: Could not set device breakpoint
Iam not able to debugg properly
Sini,
The MSP430, like any other microcontroller,has a limited number of breakpoints. Some of these are used to break at main and other locations. I suggest you disable all your own breakpoints and run it again.
Please tell us about the debugger you're using (CCS, IAR, CrossWorks, etc) as well as the MSP430 you're using.
Regards,
Gustavo
iam using CCS.I have tried many times disable the break point and and put it back
what iam facing the problem means inside the switch case its not executing the proper staements.debugg point is excuting some wrong statements
Are you now able to debug correctly and set breakpoints? Not sure what you mean by this
sini sebastian said:what iam facing the problem means inside the switch case its not executing the proper staements.debugg point is excuting some wrong statements
psa said:Are you now able to debug correctly and set breakpoints? Not sure what you mean by this[/quote]what iam facing the problem means inside the switch case its not executing the proper staements.debugg point is excuting some wrong statementsIt is possible that due to code optimization the line where the breakpoint shall be set has been moved out of the case block (common subexpresseion elimination) or even has been eliminated totally (e.g. a redundant write or an assignment that isn't use anywhere later).
In this case, the debugger is unable to locate the code that belongs to a certain code line, or the proper code line for the current execution point, either due to ambiguity or due to no code generated.Disable compiler optimization and try again. But be aware that thsi will generate larger and slower code.
**Attention** This is a public forum