This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm testing code using an MSP430F26x timer to capture the tick count of an input signal using timer B. Timer B clock is a 10 kHz clock and Timer B tick count max is 10000 which rolls over every 1 second. The input signal is a 1 Hz external signal and its capture count is read every second by the code running on TBCCR2.
The following timer register setting is being used: MOV #CAP+CM_1+SCS+CCIE, &TBCCTL2
Sometimes an issue is seen where that the capture tick count register content oscillates between two adjacent ticks over several reads. So TBCCR2=10 is read at time N seconds and then TBCCR2=11 is read at time N+1 seconds followed by TBCCR2=10 being read at time N+2 seconds and so on for some seconds.
I'd like to find out if this TBCCR2 oscillation could be happening because the 1Hz input signal occurs exactly at or slightly after 10 timer B ticks after timer B starts counting every second. I'd also like to find out if there's any way to mitigate this behavior of the MSP. Please let me know.
Thanks.
My first guess is the DCO clock modulator, which introduces jitter to fine-tune the (average) clock speed. The jitter pattern repeats every 32 "ticks", but if SMCLK/10kHz isn't a multiple of 32 the final timer tick will fall in a different place in the clock tick pattern each second. Of course, if you turn off the modulator you lose your calibrated SMCLK speed.
I think if you quadruple the Timer tick rate and quarter the captured count, you will get comparable results with less jitter.
That is, clock the Timer at 40kHz from 0 up to 39999 and roll over every 1 second. When a count is captured in CCR2, shift it right 2-bits and take that as your result.
No, under this circumstance the DCO clock has nothing to do with it.
By the way, how stable is your 10 kHz used to clock the Timer? How stable is your 1 Hz being captured by the Timer? Can that be the cause of variation of captured counts? In that case, the variation is real and what I suggested previously will not be able to reduce that variation.
The behavior (timer capture tick oscillating) is similar between the two cases of the SCS bit being cleared/set, but occurs at different edges of the timer input clock.
I mean that in one case the timer capture tick count varies when the captured signal is aligned with the rising edge of the INCLK, while in the other case the timer capture tick count varies when the captured signal with the falling edge of the INCLK. So depending on the phase offset between the captured signal and the timer clock (0 delay from INCLK rising edge or 1/2 clock delay from INCLK rising edge) the behavior shows up at different times.
This seems to be similar to a quantizer output where the analog input offset could be set. So the digital output LSB could represent either (a) analog values between -1/2 and +1/2 of first quantizer step or (b) analog values between 0 and 1st quantizer step.
If either the 10 kHz clock or the 1 Hz signal has a 50 parts per million variation, you would expect the captured counts to vary by 1 count within a couple of seconds.
You said they are "stable". Do you mean down to 1 part per million? Or better than that?
**Attention** This is a public forum