Hi.
On MSP430F5232, I am planning to use “4-pin JTAG mode”. I want to confirm which signals need to be used to enable this mode. Beside four JTAG signals (TDO, TDI, TMS, TCK), two control signals seem to be the right ones: RSTDVDD/SBWTDIO & TEST/SBWTCK.
I believe I need to use TEST signal for sure. How about SBWTDIO signal? The description in the datasheet (SLAS897-Sept.2013) says “SBWTDIO is required to interface with MSP430 development tools and device programmers”. So, do I need to control SBWTDIO from the FPGA as well as TEST signal?
By the way, there a description on this issue in the forum’s thread called “MSP430F5510 4-wire JTAG entry sequence question”. It says “The 4-wire JTAG interface access is enabled by pulling the SBWTDIO line low and then applying a clock on SBWTCK (TEST).” Does it mean that “pulling SBWTDIO low” is a pre-condition of enabling 4-wire JTAG interface? If so, can I simply tie SBWTDOP to the GROUND while routing TEST (SBWTCK) to the FPGA?
Thank you.