This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

issue using callibrator.exe for msp430f47197 three phase energy meter

Other Parts Discussed in Thread: MSP430F47197

i m working on msp430f47197. i make evalution board of three phase energy meter n   m using ccs. i can get correct data on hyperterminal. now i want to calibrate my meter using ' slaa409a ' GUI --> callibrator.exe  .... but it is not working. i can not get green light..

when i m loading source code which is given by TI on IAR embedded workbatch then i GUI is working..

and my code is different than ti source code.....so i wnt help regarding this topic....how can i callibrate ?? 

  • when i use my ccs code in IAR then i m getting this type of error which is shown below..my ccs code is working perfectly but juzz i cant get any responce in callibration.exe  so i m trying this way.... plz help  me

    Building configuration: sum4 - Debug 
    Updating build tree... 

    21 file(s) deleted. 
    Updating build tree... 
    Emeter_Calib.c 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 89 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 90 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 91 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 102 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 103 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 104 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 116 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 117 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 118 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 175 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 183 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Calib.c 190 
    Emeter_Display.c 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Display.c 370 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Display.c 385 
    Emeter_EEPROM.c 
    Emeter_Hilbert_Correction.c 
    Emeter_Init.c 
    Emeter_Interrupts.c 
    Emeter_Main.c 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Main.c 1012 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Main.c 1338 
    Warning[Pa093]: implicit conversion from floating point to integer C:\Documents and Settings\fin_20para\Emeter_Main.c 1365 
    Emeter_MD.c 
    Emeter_RTC.c 
    Emeter_Soft_I2C.c 
    Linking 
    Error[e16]: Segment INTVEC (size: 0x36 align: 0x1) is too long for segment definition. At least 0x16 more bytes needed. The problem occurred while processing the 
    segment placement command "-Z(CODE)INTVEC=FFE0-FFFF", where at the moment of placement the available memory ranges were "CODE:ffe0-ffff" 
    Reserved ranges relevant to this placement: 
    ffe0-ffff INTVEC 
    Error while running Linker 

    Total number of errors: 1 
    Total number of warnings: 17

  • are you sure that your port settings at the calibration-config.xml are right? and the same with the settings of your serial port at device manager?
  • George Papakonstantinou said:
    are you sure that your port settings at the calibration-config.xml are right? and the same with the settings of your serial port at device manager?

  • yes it was one year ago.But maybe there will be users that may face the same problem in the years to come.

**Attention** This is a public forum