This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
Today I wanted to play with the MSP-EXP430FR5739 experiment board, but the CCS said:
Could not find MSP-FET430UIF on specified COM port
I tried to connect it to an another USB port, reinstalled CCS, rebooted the pc a few times, reinstalled the device driver, but none of these solved the problem. I searched the forum, but I only found answers like: stop another programs, reboot, reinstall etc.
The MSP430FR5739 uC on the panel is working, I tested it with an another programmer (F5529 launchpad).
I think the on-board programmer is dead. The ICs are not hot, and there is no smoke :) so I think it is a software fault.
How do I make sure that the programmer is dead? And how can I solve this problem?
IDE: CCS 6.0.1
OS: Win7 x64
Thanks
**Attention** This is a public forum