Hi All,
Is there any way to generate a different output format in IAR kickstart version? It only let's me generate the .d43 file, any other I try it gives me the error "Can only generate UBROF output from these files". I would like to generate any other type of Hex file, like intel-hex or ti-txt. I read some documentation on IAR supp.iar.com/FilesPublic/UPDINFO/004843/xlink.ENU.pdf
It says that the error is that the demo version I am using is can only generate UBROF output, that I should use a Kickstart or full version, but I am using a kickstart version, I know is like a demo version because of the code size limitations, but then the documentation is not clear, as it says that a kickstart version should be able to generate other output formats. Any of you have had this problem? is there any solution to it?
regards,
mx_de