hai,
I'm somewhat new to programming microcontrollers. I've taken a course on programming an MSP430, but I was using a different kit then, and now I am working with the ez430-RF2500 development kit. I'm having a lot of trouble understanding, especially the wireless communication. I've never dealt with wireless microcontroller programming.
And please try and be patient with me, again I'm quite new so you can expect stupid questions from me on this issue.
my question is, it's a very simple one.
i made a simple transmission and reception code for ez430-rf2500. It is not responding with "IAR workbench kickstart for msp430 4.21" and also with "IAR workbench kickstart for msp430 5.30". It shows error in the header itself. so please give me the correct need to be installed for programming