This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EZ430-RF2500
Hello all,
I'm working with the EZ430-2500T and both IAR and CCS to see which I like better. For IAR: in the project options window, under the "target" tab there is a list of MSP boards you can select, but ez430-2500T is not one of the listed options. Is there a better choice that I should have selected besides "Generic MSP430 device?
For CCS, when you create a new CCS project, which board do I select from the dropdown box that defaults to "Generic ARM7 Device"? Same question as above I guess.
Thanks in advance!
James
**Attention** This is a public forum