This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F149 UART-Idle-Line Multiprocessor



I can not get   URCTL:BRK  -flag and no interupt occur  after last reciving byte + 10bits(==1's) + any time more
all data bytes are reciving correctly (without any error)

I do:

main() { ... U0CTL=SPB|CHAR;  ...  ;  for(;;) {...  ;  U0RCTL = URXWIE|URXEIE; .... ;  LPM3 ...};}

interrupt[VECTOR_RX] void uart_rx (void)
{
  if (U0RCTL&RXERR    ) return;
  if (U0RCTL&RXWAKE ) {  if  (RXBUF0==cADR)  U0RCTL&=~URXWIE; return;  }
  buffer[++byte_cntr] = RXBUF0;
}

  • I'm sorry, I precise my script:

    main() { ... U0CTL=SPB|CHAR;  U0RCTL = RXERR|BRK; ...  ;  for(;;) {...  ;    if (U0RCTL&BRK) { ....; U0RCTL=URXWIE|URXEIE; ME1|=URXE0; IE1|=URXIE0;....; }  ....LPM3 ...};}

  • Unfortunately I realized my mistake: Break condition and Idle line condition are not the same.
    Break condition used (for example) for DMX-protocol
    I need identify end of reciving paket by idle line condition (MODBUS-protocol)
    Using of timer tick - it is a single way? No UART-hardware support?

  • I need interupt after last data byte transmited (complite shift register output, no new data in tx-buffer).
    Can I use TXWAKE and put one more byte (dont care byte), when last valuable byte in shift register?
    I test this: but "dont care byte" has been appeared in output, why?

  • Why there is no info in datasheet  about:

    if (P3SEL&BIT4)==0     UART0 TX is disabled (like ME1&=~UTXE0)

    Maybe I have mistake?

  • Please give me sure about:

    if  ( ME1.UTXE0==0  &&  P3SEL.4==1) 
    than   P3.4  will work as input (regadless  P3DIR.4 or not)

  • Don't worry about all of my questions above.
    I found answers (all problem is my mistake)

    I should notes about lack of information

    UART-TX is full empty, after writing 1 byte to TX-BUFFER:
        - UTXIFG0 going to 0
        - time (~ about one transmitting-bit)
        - UTXIFG0 going to 1

    There is no this information in datasheets, but it is necessary!!

  • You can use teh ARDY(IFG/IE) interrupt. It is flagged when the last transmission has been finished, based on the configuration. So it should happen if the last byte has been sent and TX buffer is empty.

    Of course your 'don't care' byte is being sent, as the hardware does not know that it is a don't care byte :)

     

     

     

  • Hardware know about "dont care byte"
    because TXWE-bit has been set,
    before "dont care byte" has been pushed into TXBUF

    In this case TX-output stay in "idle-line state"
    instead of trasmitting "dont care byte" wich has been pushed into TXBUF.

    This work properly
    I did mistake when set TXWE-bit into wrong address (special function register)

**Attention** This is a public forum