Other Parts Discussed in Thread: MSP430F5510
We recently had a failure of the UART RX (pin1.1). There appears to be a low impedance path to ground which causes the voltage to drop to around 0.7V (3V expected) while connected direclty to the output of another micro (MSP430F5510). When connected to a 3V source directly it sinks about 40mA into the pin, so it appears as though the impedance is less than 100Ohms. However, when I probe with a DMM the resistance to ground is on the order of 45-50kOhms.
There are no current limiting ressitors or ESD clamping diodes connected to this pin and I suspect the failure is due to ESD damage during handling. My question is if the failure mode is consistent with ESD damage, or if it could be something else.