This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have purchased mspfet recently . I plugged in the device at the v first time it installed drivers and firmware upgrade . then i connect the debugger to the target device ,tried to connect Its showing the following error. I was using MSP430FET UIF earlier and now mspfet . I hope the 14 pin connector is the same . I am using CCS6.0 as well CCS5.5.
Drivers have installed properly and showing the detection in device manager .
Now what to do ?
Regards,
Apurwa
**Attention** This is a public forum