This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am designing a new MSP430 board, and I am considering leaving off the LFXT to save space. However, I want to use the UART BSL as the firmware update interface.
Will the BSL work without LFXT? I read the data sheet, the UG, and the BSL UG, and none of these documents give the clock requirements for the BSL (or at least I couldn't find it). What clock does the BSL use?
Mr. Gross,
Many thanks. I designed the boards, and now have them in house. Unfortunately, the UART BSL does not appear to respond. I am using the BSL scripting tool, and I've also poked around a bit with RealTerm, and haven't gotten a byte back from the MSP430.
Are there any debug pins so I know that it's alive?
I've checked all the obvious problems (Vcc ok, pinout), but is there something else I should look for?
I'd hate to have to solder in a JTAG connector to program the board...
Regards,
Bill
**Attention** This is a public forum