This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have received the inquiry from my customer.
Device : MSP430F6433IPZ
(1) DVCC1 (pin 25), DVCC2 (pin 64), and DVCC3 (pin 89) have prepared a three-place pin, in order to secure internal current distribution.
For that reason, as for these three pins, the inside is connected in common.
Is this right?
(2) The inside is connected in common DVSS1 (pin 26), DVSS2 (pin 63), and DVSS3 (pin 90) similarly.
Is this right?
(3) Moreover, AVSS1 (pin 12), AVSS2 (pin 15), and AVSS3 (pin 83) are similarly connected inside.
Is this also right?
(4) DVSSn (digital GND) and AVSSn (analog GND) are not directly connected inside.
Is this right?
Regards, Hidetaka.
**Attention** This is a public forum