This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm porting Pervasive Displays code for their Extension Kit, http://www.pervasivedisplays.com/kits/ext_kit, from MSP430F5529 to MSP432P401R.
MSP430 has an intrinsic __delay_cycles(). I looked for equivalent one in MSP432 but found none. Is there any ? If not what are the workarounds ?
One possible solution is use MSP432's intrinsic of sleep() and a timer but I want to avoid that because I don't want to use up the timers.
The TI ARM v5.2.x compiler does support a _delay_cycles
() intrinsic, which I have used on other ARM devices such as a Cortex M4F Tiva device, so should work on a Cortex M4F MSP432 device.
One issue I found was that on some ARM devices was that the actual delay could be several times that requested and could change according to the code alignment - see What is its unit of number of _delay_cycles()
i.e. using _delay_cycles() can be difficult to generate a deterministic delay, even when no interrupts are occurring..
Hi Tao,
We do not support this intrinsic in GNU(gcc) or IAR. So you will have to implement it yourself.
This is what I use:
#include <stdbool.h> #include <stdint.h> #include "driverlib.h" #include "demo_sysctl.h" //***************************************************************************** // //! Provides a small delay. //! //! \param ui32Count is the number of delay loop iterations to perform. //! //! This function provides a means of generating a delay by executing a simple //! 3 instruction cycle loop a given number of times. It is written in //! assembly to keep the loop instruction count consistent across tool chains. //! //! It is important to note that this function does NOT provide an accurate //! timing mechanism. Although the delay loop is 3 instruction cycles long, //! the execution time of the loop will vary dramatically depending upon the //! application's interrupt environment (the loop will be interrupted unless //! run with interrupts disabled and this is generally an unwise thing to do) //! and also the current system clock rate and flash timings (wait states and //! the operation of the prefetch buffer affect the timing). //! //! For best accuracy, a system timer should be used with code either polling //! for a particular timer value being exceeded or processing the timer //! interrupt to determine when a particular time period has elapsed. //! //! \return None. // //***************************************************************************** #if defined(ewarm) || defined(DOXYGEN) void SysCtlDelay(uint32_t ui32Count) { __asm(" subs r0, #1\n" " bne.n SysCtlDelay\n" " bx lr"); } #endif #if defined(codered) || defined(gcc) || defined(sourcerygxx) void __attribute__((naked)) SysCtlDelay(uint32_t ui32Count) { __asm(" subs r0, #1\n" " bne SysCtlDelay\n" " bx lr"); } #endif #if defined(rvmdk) || defined(__ARMCC_VERSION) __asm void SysCtlDelay(uint32_t ui32Count) { subs r0, #1; bne SysCtlDelay; bx lr; } #endif // // For CCS implement this function in pure assembly. This prevents the TI // compiler from doing funny things with the optimizer. // #if defined(ccs) __asm(" .sect \".text:SysCtlDelay\"\n" " .clink\n" " .thumbfunc SysCtlDelay\n" " .thumb\n" " .global SysCtlDelay\n" "SysCtlDelay:\n" " subs r0, #1\n" " bne.n SysCtlDelay\n" " bx lr\n"); #endif
Best regards,
David
**Attention** This is a public forum