This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a brand new MSP-FET. Windows XP 32 install drivers without problem, but I can not make it to work in Windows 7 x64.
7 shows it as a "MSP Tools Driver" in device manager and it can't find drivers for it. I have tried last versions of CCS, IAR, MSP Stack and standalone drivers package. No solution. Windows 7 can't find any compatible hardware drivers.
Any clue?
Hello,
I have done already.
I have tried the CCS, IAR, MSP Debug Stack and the standalone installer drivers. All latest version. No luck.
I have forced installing the drivers selecting "MSP Tool Drivers" from device manager and assigning manually drivers. System complains but installs them. But then I only have "MSP Application UART1" and CCS can't find the FET.
I have installed it correctly on Windows XP and CCS have just update it's firmware.
On Windows 7 x64, in device manager, the MSP-FET appears as
USB\VID_2047&PID_0014&REV_0200
USB\VID_2047&PID_0014
and none of them appears in the inf files.
I'm lost. Never had a problem like this with an USB device.
**Attention** This is a public forum