This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
I got MSP432 launchpad a week ago.
Studying MSP430 LaunchPad Workshop Course Workbook as my textbook. There was no problem whatsoever. But in lab 7(Energy trace) I've encountered a problem.
After flashing solution of lab_07b_lpm_timer project. I ran EnergyTrace. But EnergyTrace immediately stops and it says "Target current exceeded with the maximum current (75mA) supported by EnergyTrace."
Huh?
So I actually measured current and voltage with my multimeters and the uc was drawing 170 mA. Even in the reset state.
No external circuitry has ever connected to my launchpad. Even no single jumper wire.
What could be a cause of this problem? ESD?
-----------------------------------------------------------------------------------
Sep. 3,
Planning to get another MSP432 LaunchPad and MSP432P401RIPZ(LQFP100) next week.
I will update this post after replacing MSP432 chip on this LaunchPad board.
Thanks to everyone who cared about my problem.
-----------------------------------------------------------------------------------
Sep. 10,
Replaced old MSP432 with the new one. It turns out that the MSP432 was the problem. After replacing, current consumption of the board drop to 1.5 uA, with debugger connected and all default jumpers connected. Very happy with it.
Yes. I used that header pins for the measurement.
This is my measurement setup. lab_06c: Timer directly drives LED is running.
Left meter: measuring current in Amps range.
Right meter: measuring voltage of 3v3 rail.
No 90º jumpers.
FYI. surface temperature of the MSP432 chip was about 52 ℃ (126℉). delta T ≈ +29 ℃
Dung,
Sure.
I did experiments you said.
Not pictured but removing jumpers while running blink program did not affected to current readings. Just LED current fluctuations are gone. Still around 170 mA.
I imported LPM3 example to my workspace and flashed to MSP432. Example from "MSPWare: msp432p401_pcm_02 Enter LPM3 (ARM Deep Sleep Mode) with ACLK = REFO"
Also every jumpers are removed.
Curiously entering LPM3 drew more current. it's 190 mA now.
While pressing reset button 170 mA.
Video:
Hi Sebastian,
I don't have access to professional thermal imaging cameras. Instead I have small smartphone attachable thermal camera. - Seek Compact XR from Seek Thermal, Inc.
Resolution is not that high, manual focus, no colorbar, app has some bugs, but kinda works.
Condition: Same as before
Again, LPM3 example program.
3.3 V Externally powered through J6.
All jumpers removed.
Set JTAG selection switch to external.
0:03 Power on - 197 mA @ 3.27 V
3:04 Close up board inspection
3:56 Power off
No external sign of short. Hmm.
Definitely some kind of bad things happened to the silicon in my chip as Dennis said.
Thanks,
Seungwon
WOW! That comes from a smartphone?! It is great!
But desoldering the MSP from the LaunchPad isn't worth the effort, I guess :-\
I'm sending you a PM to get your address information to send you a new unit. I will also send you a prepaid label to ship your current unit back to me for evaluation.
Anyone encounters the same problem? I am seeing about 190mA too, but i can still program and the MCU still work.
**Attention** This is a public forum