Hi,
I need to buy an evaluation kit for MSP430FR2033 to drive a SPI controlled DAC and also some external switches using the GPIO's of MSP430FR2033.
Which evaluation kit should i go with ?
Thanks in advance
Nithesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need to buy an evaluation kit for MSP430FR2033 to drive a SPI controlled DAC and also some external switches using the GPIO's of MSP430FR2033.
Which evaluation kit should i go with ?
Thanks in advance
Nithesh
Hi Nithesh,
You have a couple of options. The easiest (and probably cheapest) is to buy a FR4133 LaunchPad and use it. The FR4133 and FR2033 are very similar parts, with the FR4133 having extra features that you might not need or care about (such as the LCD controller). Alternatively, you could buy the FR2033 Target Board and use it, but it is significantly more expensive than the LaunchPad. Depending on your needs/requirements, one of the two options listed above will work for you.
Mike
Hi Mike,
Thank you for your reply. I have placed an order for MSP-EXP430FR4133 launch pad.
Best regards
Nithesh
**Attention** This is a public forum