This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there,
I'm a MSP noobie trying to get a TCA8418 to talk to the G2553 through I2C. I'm using the example code given by TI:
http://www.ti.com/lit/an/slaa382a/slaa382a.pdf
..and was told I needed to rename the SDA/SCL pins in the header file. I just wanted to confirm that I am interpreting the datasheet right when modifying the code:
...and my resulting code:
Just wanted to rule out any mistakes. Any help would be greatly appreciated, thank you!
Best,
Oscar
Hi Oscar!
Beside from Clemens' answer there is another general mistake in your code:
UCB0SCL is at P1.6 and UCB0SDA is at P1.7 and in your code you write 0x06 and 0x07, but this is wrong. 0x06 means Px.1 and Px.2 (both together). 0x07 means Px.0 and Px.1 and Px.2 (again together). You want 0x40 for Px.6 and 0x80 for Px.7 - look here:
BIT0 BIT1 BIT2 BIT3 BIT4 BIT5 BIT6 BIT7 0x01 0x02 0x04 0x08 0x10 0x20 0x40 0x80
And of course you can combine them - for Px.6 and Px.7 you do
0x40 | 0x80 == 0xC0
Dennis
**Attention** This is a public forum