I used IAR to compile and debug and also load the firmware into MSP430F47197. Also, recently I've learnt to load the firmware through the JTAG using the MSPFlasher! (without using IAR) And as my MSP has not FRAM I cannot use (-p) command for protection!
Now, here is the question: In order to protect the MSP against getting programmed and further load the firmware what shall I do?
As I might need to apply some changes in the future let's say in 2 years, I do not want to blow the fuse. So, I believe the only option is having a password! But where?! In the firmware?!!!
Not to mention that the IAR that I use, its password protection option is disabled! (As you can see through the picture below)
Any idea or thought appreciated!