Hi Dear,
I have few questions about MSP430F6438 MCU. Is there some one know answer.
Q1. If the extra OSC (32khz to XT1) must works, before I program the MCU by JTAG interface. Which one is a define clock source in MSP430F6438?
Q2, Do it need external capacitors, if I use a 32khz crystal on XT1 for MSP430F6438.
Q3, If the external capacitors is necessary, would you know how much pf it is.
I read the datasheet of MSP430F6438, it said put a 32khz crystal on XT1 without any extra parts. I did like that, but it did not works. I read the Application Report-SLAA322B-MSP430 32-kHz Crystal Oscillators, it said MSP430 family need extra capacitors difference capacitors depend on MSP430Fx. I try it too, but it is still did not work. So I have Q2 and Q3.
I note some discussion online which are about how to setup the OSC of MSP430 MCU. So I have the Q1.
Is there some one can give me answer.
Thanks,
Dison