This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I'm using MSP430F5419A for the development. Currently I use a external 32768Hz oscillator connected at XT1, what's the max frequency I can setup for MCLK?
Download code examples www.ti.com/.../slac375 and check msp430x54xA_UCS_x files for DCO setup.
MCLK can go over 25 MHz, but from my experience using directly XT2 for overclocking is better choice. I am running some MSP430F5510 boards at 48 MHz MCLK directly from XT2 48 MHz crystal.
http://forum.43oh.com/topic/3909-msp430f550x-based-logic-analyzer/?p=69255
**Attention** This is a public forum