Hello,
In the IC description on: www.ti.com/.../msp430f2112
says: 16-bit Ultra-Low-Power Microcontroller, 2kB Flash, 256B RAM, 10 bit ADC, 1 USCI
However at page 15 It can be read:
USCI_A0 provides support for SPI (3 or 4 pin), UART, enhanced UART, and IrDA.
USCI_B0 provides support for SPI (3 or 4 pin) and I2C
Does it have 2 independent modules?
I need simultaniusly I2C and UART. Is it possible with MSP430F2112 ?
Many thanks
BR