This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 Stand Alone without any external circuitry and timers?

Other Parts Discussed in Thread: MSP430G2553

It's been about 4 years since I've touched my MSP430's but I now have a perfect application for them.  They are being used in a 'light' gun, where if a button is pressed, I set a pin high for 50 ms, then low and sleep for 50 ms, then resume in the loop (so you can only shoot a limited amount of times / second).  I have 2 Launchpads, so could I just program them on those, and just wire the buttons to IO pins and do digital reads without any issues? I ask because the Arduino says to use a crystal if in stand alone.

Thanks.

**Attention** This is a public forum