This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The MSP432P401 data sheet specifies an HF crystal ESR range of 15-30 ohms. I have not been able to find the Geyer crystal specified in the data sheet at any U.S. distributor. I would like to find an alternative component available from Mouser if possible, but I can't find a 48MHz crystal from any manufacturer specifying ESR less than 50 ohms at 48MHz. The Geyer data sheet does not specify ESR, only a series resonance value, which is 50 ohms at 48MHz.
Mouser stocks 185 different SMD 48MHz crystals meeting my operating temperature range, and none of them meet the TI spec for ESR. I can't believe TI would make a microcontroller that will only work with a Geyer crystal, but I'm not finding any other options. I need the oscillator to start up reliably from -40 to +70 C. Any advice?
As I know in most cases DCO is usable without external HF crystal. But if needed I recommend using EPSON crystals because of low tolerance to PPM. But it costs a little bit more because of high precision. ESR of crystal changes in different operational modes. And ESR of ESPON 48 MHz 10 ppm crystal has maximum documented ESR of 60 Ohm at 54 MHz. This is only a recommendation from low practical skilled user. Refer to TI special publications about crystal selection.
Low PPM is indicated under referenced temperature of +25 deg.C. None of crystals on a market can provide such precision in all temperature range.
Thank you for the reply. Please post a note when the revised datasheet is available.
Regards,
Clay
**Attention** This is a public forum