This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to use a MSP-EXP430G2533 Launchpad to program the processor and then remove the processor and use it in a stand alone circuit. When I power up the processor in the stand alone circuit, it does not appear to be functioning. Do I need to use the Xin and Xout with an external crystal in order for the processor to operate? Looking at the Launchpad board, it does not appear that a crystal is present although there are resistors in the leads out of the processor. I guess my question is -- how do it make the chip work outside of the Launchpad environment?.
Any help will certainly be appreciated.
Dear Fred,
already answered above, but I like to repeat:
Pls check document
on page 23 and others - other pages, other documents.
A high frequency crystal is used for processor control directly made from xtal. A 32kHz crystal is used for frequency multiplications and PLL/DCO applications, and calibration data for DCO let run the oscillator without any xtals.
Happy coding!
Bernd
**Attention** This is a public forum